MITSUBISHI ELECTRIC Changes for the Better
Sustainability

Smart Energy Management in Modern Manufacturing: How Innovation is Transforming Industrial Efficiency

14.04.20254 min read

In the ever-evolving world of manufacturing, energy efficiency is no longer just an option - it’s a necessity.

With rising energy costs and stricter environmental regulations, manufacturers are actively seeking intelligent energy management solutions that optimise consumption without compromising productivity. Mitsubishi Electric’s EcoAdviser is at the forefront of this transformation, demonstrating how AI-driven analytics and real-time monitoring can revolutionise industrial energy management.

          The Next Generation of Energy Management Systems

          Unlike traditional monitoring tools that simply track energy usage, EcoAdviser goes beyond basic data collection. It employs advanced AI diagnostics to detect inefficiencies, predict potential issues, and recommend actionable improvements. This proactive approach allows manufacturers to reduce energy waste, lower operational costs, and enhance overall efficiency without requiring complex manual interventions.

          Real-World Impact: Success at Fukuyama Works

          A prime example of EcoAdviser’s capabilities in action is its implementation at Mitsubishi Electric’s Fukuyama Works facility. Specialising in circuit breakers and measurement and control devices, the factory faced significant energy challenges—particularly in its moulding operations.

          Through EcoAdviser’s intelligent visualisation capabilities, facility managers identified the curing furnaces as the primary source of excessive energy consumption. AI-driven diagnostics revealed two major inefficiencies: 

          • Early furnace startup: The furnaces were switched on at 7:00 AM, despite production not beginning until 11:00 AM, leading to unnecessary energy waste.
          • Uneven energy distribution: One furnace was consuming three times more energy than others due to a misaligned exhaust damper, resulting in substantial heat loss.

          By adjusting startup times and repairing damper systems, the factory achieved annual energy savings of approximately 1.4 million yen, demonstrating the real-world impact of intelligent energy management.

              Leading-Edge Motor Technology: The EM-A Series

              Beyond smart monitoring, energy efficiency in manufacturing also depends on the motors that drive production equipment. Mitsubishi Electric’s EM-A Series represents a revolutionary leap in motor design, integrating permanent magnet technology with a patented salient-pole core to maximise efficiency and reduce energy loss.

              Key Innovations in the EM-A Series:

              • Sensorless Control: The innovative rotor design eliminates the need for traditional encoders, simplifying system complexity while ensuring precise speed and position control.
              • Energy-Efficient Performance: The salient-pole core configuration provides variable motor inductance, enhancing energy efficiency across different load conditions.
              • Versatile Applications: Ranging from 0.1kW to 3.7kW, the EM-A Series is suitable for compact, high-precision tasks as well as heavy-duty industrial operations.

              Data-Driven Diagnostics: Predictive Energy Monitoring

              One of the most significant advantages of modern energy management systems is their ability to serve as predictive diagnostic tools. Unexpected spikes in energy consumption can indicate mechanical wear, system inefficiencies, or impending equipment failures. With EcoAdviser’s real-time analytics, maintenance teams can detect and resolve potential issues before they lead to costly breakdowns, improving overall system reliability.

              The Power of AI-Driven Data Analytics

              Energy management is no longer about reactive monitoring—it’s about proactive optimisation. AI-powered platforms like EcoAdviser leverage machine learning algorithms to analyse vast datasets, detecting hidden inefficiencies and providing actionable insights that manual monitoring simply cannot match.

              By identifying patterns and anomalies, these systems enable manufacturers to fine-tune production schedules, optimise machine usage, and reduce unnecessary energy expenditure.

              Seamless Integration with Factory Systems

              One of the key strengths of EcoAdviser is its seamless integration with existing factory management systems. When combined with other tools, manufacturers gain a comprehensive, facility-wide view of energy consumption, ensuring that efficiency becomes an integrated component of the entire production process.

              The Future of Sustainable Manufacturing

              As the manufacturing sector advances towards Industry 4.0, intelligent energy management solutions will play an increasingly vital role. The combination of AI-driven analytics, real-time monitoring, and next-generation motor technology provides a comprehensive strategy for reducing energy costs and achieving sustainability goals.

              The success of EcoAdviser and EM-A Series motors at facilities like Fukuyama Works proves that these are not just theoretical innovations—they deliver tangible, measurable improvements.

              By embracing smart energy management, manufacturers can not only cut costs and enhance efficiency but also contribute to a more sustainable and environmentally responsible industrial future.

              Enjoyed this article? Read more in The Art of Manufacturing Monozukuri magazine: Explore the latest edition


              Similar Articles


              Topic

              Sustainability